SKF Logo Black

Want your machines to perform better? Don’t change oil

What if you could get cleaner oil in your application without having to change it? With RecondOil Box from SKF, you can use the same oil over and over again. In fact, you can get cleaner oil than ever before. Your machines can perform better, and at the same time, your oil can be transformed from a costly CO₂ footprint into a sustainable asset. Don't change oil. Change to circular use of oil.

Contact me

#circularuseofoil

SKF RecondOil Box makes it possible to use the same oil over and over again

Circular use of oil offers several benefits

 

Sustainability improvement

  • Reduced CO₂ impact
  • Reduced energy consumption thanks to less friction
  • Reduced consumables use

Total oil cost reduction

  • Reduced costs for purchasing oil
  • Reduced costs for shipment, storage and disposal of used oil
  • Reduced costs for oil-related maintenance and production stops

Performance improvement

  • Improved system performance
  • Higher availability of the machine
  • Higher productivity

 

*CO₂ reduction when compared with traditional oil cycle. Source: Life cycle analysis performed by IVL Swedish Environmental Research Institute (2021)

Explore the range

Solutions built on the same proven depth-filtration technology, designed for different operating environments. Both deliver exceptionally clean oil through continuous filtration. The difference lies in where they are used and how the system is controlled.

 

 

Download brochure

 

3100 series

Optimised for indoor environments with digital monitoring and operational insight.

Best suited for: Indoor manufacturing and automated production environments.

2100 series

Built for demanding environments. Fully analogue, streamlined design with minimal electronics.

Best suited for: Heavy industry, mining, cement, power generation.

2100 ATEX

Designed for explosive and hazardous environments.
ATEX-certified for safe operation.

Best suited for: Oil and gas, power generation, hydrogen, metals.

Oil accounts for 5% of your maintenance budget. But affects 40% of maintenance costs

Today, most companies use their industrial oil until it degrades. This means that the oil eventually needs to be discarded and replaced with new oil. But since application owners want to get the most out of their oil, machines are often run with contaminated oil for long periods – a common cause of premature equipment failure.

  • In fact, lubrication (and lubrication-related activities) can impact more than 40% of your total maintenance budget in things such as:
Replacement of worn spare parts and components (bearings, chains, motors, pumps, hydraulic components etc.)
Increased maintenance staff costs due to machine failures and more maintenance stops.
  • In other words, you have a lot to gain by constantly keeping the oil clean. Your machines run better, live longer and become more productive with less downtime. That means less repairs and component purchases.

 

Contact me

Proven in real applications

SKF RecondOil solutions are delivering measurable results in industrial operations worldwide. From reducing varnish-related failures to extending asset life, RecondOil Box improves reliability while supporting sustainability goals.

Backed by research and technology

• Proven performance of DST-enabled systems
• Insight into nano-level contamination and degradation
• Lifecycle cost benefits

 

What our customers achieved with the RecondOil Box:

Longer machine life

Fewer unplanned shutdowns

Reduced oil consumption

More predictable performance

Lower environmental impact

Explore our knowledge hub now

Access case studies, white papers and expert insights that help you understand and implement circular lubrication in your operation.

One system – three functions

The RecondOil Box is an enhanced offline oil cleaning system that incorporates RecondOil’s patented Double Separation Technology (DST). It features a chemical/mechanical separation process which is not limited by filter pore size, and there is therefore no lower limit on the size of particles that can be removed from an oil.

We can get rid of the nanoparticles – and all other particles as well, for that matter.

With its DST filter, the RecondOil Box also removes both soluble and insoluble varnish, thereby avoiding clogged systems. 

In addition, the RecondOil Box is also efficient at water removal, and can remove dissolved, emulsified and free water out of an oil.

By reusing the oil you solve your smallest problem

The lifetime of oil is influenced by contamination – if left unchecked in a system, the contaminants cause the oil to continually degrade, until it is no longer functional. 

  • Nano-particles
  • Varnish
  • Water

We make it easy not to change oil

In one compact system, easily installed to your application, you get continuously clean oil, resulting in reliable and stable processes. 
The RecondOil Box is also an investment with a short payback time, offered at a fixed monthly cost, where you can choose between different service packages. In addition to the Box itself, the packages can include everything from commissioning, new filters, technical support, and oil condition monitoring of your oil.

Curious about the details?

Discover how SKF RecondOil supports circular oil use across different applications and environments. These brochures cover the RecondOil Box family, circular oil use, and certified solutions for hazardous environments.

 

 

Meet the Recondoil Box
family

View Brochure

 

Turn your oil into an asset
with RecondOil Box

View Brochure

 

Circular oil use in
hazardous environments

View Brochure

 

I want to know more

SKF RecondOil enables you to use the same oil over and over again, extending the lifespan of your industrial oils almost endlessly.